Technical FAQs

Ask a Question

Does Vijeo Designer supports X-Y Graph?

Yes Starting with Vijeo Designer V6.1 SP4. This new features allows to plot X and Y coordinates.

You can set up to eight block or array variables per XY Graph part.
 




 

Was this helpful?
What can we do to improve the information ?