Technical FAQs

Ask a Question

Is there a way to reset the BMXNOR0200 module to the default password of USER USER?

Yes. Using Web Designer create a project and set the target address to the BMXNOR0200. Under target properties, click the Secure HTTP button and set a new Username and Password. This will work as long as the module has a solid Run led and no error (ERR,CARD ERR or DL led) and also has valid IP address that Web Designer can connect to.


 
Was this helpful?
What can we do to improve the information ?