Browse FAQs

How do I wire a 2-wire transmitter to an Advantys STB analog current output module?

Published date: 14 February 2019

Issue:
The following wiring diagram indicates how to wire a 2-wire transmitter to the STBACO1210 or the STBACO1225 analog current output module. Loop supply voltage is provided by the PDM.


    • Pin 1 +24VDC for sensor
      Pin 2 input from sensor
      Pin 4 return from input
      Pin 6 +24VDC return

Product line:   Advantys

Environment: wiring information

Cause: not applicable

Resolution: not applicable
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.