Technical FAQs

Ask a Question

Dimensions for CM3000 mounting bracket

Issue
User would like to know the dimension or view the drawings for a CM3000 mounting bracket. 

Product Line
CM3000 Meters

Environment
Meter Mounting Hardware

Resolution
Below is an attached document that includes the drawings for the CM3000 bracket. Dimensions are detailed in the drawing as well. 

Mounting Bracket for CM3000
Please see attached pdf file for mounting bracket drawing.


 

Was this helpful?
What can we do to improve the information ?