Technical FAQs

Ask a Question

ION6200 unresponsive immediately after a power up

Issue: 
ION6200 meter becomes unresponsive. The user may notice that pressing the buttons on the ION6200 does nothing.

Product Line:
ION6200 Series Meter

Environment:
Power Metering

Cause:
The RS-485 bus may momentarily become unusable as the 6200 powers up on a rs-485 network.    This is due to hardware being in an un-initialized state until the code runs.

The RS-485 transceiver starts in transmit more and last for about 300ms.    

Resolution:
Allow 10 seconds to pass before trying to use the meter after the meter is powered on. 
 
 

Was this helpful?
What can we do to improve the information ?