Technical FAQs

Ask a Question

What are the dimensions of the Enercept Network Adapter 485 (ENA 485)?

Issue 
What are the dimensions of the Enercept Network Adapter 485 (ENA 485)?

Product Line
Enercept Network Adapter 

Cause 
User would like to know the dimensions of the Enercept Network Adapter

Environment 
Installing Enercept Network Adapter

Resolution 
Enercept Network Adapter dimensions are: 3.75 inches long, 1.5 inches wide and about 2 inches deep to compensate for the connectors and wiring.

Was this helpful?
What can we do to improve the information ?