Technical FAQs

Ask a Question

Why do I get this GFXWEB ERROR The IPLAlarmEventConnection interface can not be created, when I click on any GFX diagram screen in Web-3000?

Issue: 
Why do I get this GFXWEB ERROR The IPLAlarmEventConnection interface can not be created, when I click on any GFX diagram screen in Web-3000

Product Line
Powerlogic SMS
SMS Web3000

Environment:
System Manager Software
Powerlogic Web Client

Cause:
Unable to display GFX Diagram in SMS Web-3000


Resolution:
Run the SMS admin tool to correct the issue.
Click on Start All pPrograms/Powerlogic/Tools/Admin Utility as shown below.

 

 

Was this helpful?
What can we do to improve the information ?