Technical FAQs

Ask a Question

How do you log in as a different user when using SMS-1500, PMX-1500, and SMS-121?

Issue
customer need to know how to change user account that is logged into the system

Product Line
System Manager Software (SMS-1500, PMX-1500, and SMS-121)

Environment
User login to SMS

Cause
user interface does not have a sign off selection

Resolution

To log in as a different user, you must close the software (since there is no seperation of Server/Client) and log back on as a different user.
  • Original article#2326

    Internal PMO/PMC

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL186201 V1.0, Originally authored by KBAdPM on 07/04/2007, Last Edited by KBAdPM on 07/04/2007
Related ranges: System Manager 3.3
Was this helpful?
What can we do to improve the information ?