Technical FAQs

Ask a Question

Cannot see SQL ODBC Datasources or can see SQL ODBC Datasources but they keep failing the source test.

Product Line:
System Manger Software (SMS) 4.0

SQL ODBC Datasources

This is a symptom of the SMS Demo being installed, while trying to use a licensed version of SMS 4.0. The SMS Demo is not to be installed with ANY other SMS software.


Uninstall all SMS and DEMO software and reinstall SMS in order to fix the problem.

Was this helpful?
What can we do to improve the information ?