Technical FAQs

Ask a Question

Does the Power Meter Series 600 Display require it's own firmware?

Issue
Does the Power Meter Series 600 Display require it's own firmware?

Product Line
PM600

Environment
Firmware

Resolution
The Power Meter display works as a terminal remotely connected to the Power Meter. The firmware that tells the display what to do is stored in the Power Meter base. No additional firmware is required.

See FA313600 for the meters firmware.

Was this helpful?
What can we do to improve the information ?