Technical FAQs

Ask a Question

What are the system requirements for Unity Pro 6.0?

System requirements
 

    • System with Microsoft Windows Vista Business 32bits / Windows 7 Professional 32/64bits
      • System: Pentium Processor 2.4 GHz or higher, recommended 3.0 GHz
        RAM memory: 1GB minimum; recommended: 3GB
        RAM memory using DTM: 2GB; recommended: 4GB
        Hard disk: minimum available free space 8 GB, recommended 20 GB
        Microsoft Internet Explorer 5.5 or higher
        On Windows 7 64bits System, installation of Windows 7 Service Pack 1 (SP1) is mandatory in order to use Unity Pro V6.0
         
      System with Microsoft Windows XP Professional
      • System: Pentium Processor 1.2 GHz or higher, recommended 3.0 GHz
        RAM memory: 512 MB minimum; recommended: 1 GB
        RAM memory using DTM: 1GB; recommended: 3GB
        Hard disk: minimum available free space 8 GB, recommended 20 GB
        Microsoft Internet Explorer 5.5 or higher
         
        Windows XP in Chinese only supports use of Unity Pro V6.0 in Chinese or in English.  
     
    • DVD-ROM drive: to install the software;
      • DVD-ROM writer recommended
         
      Display:
      • Min VGA (800-600).
        Recommended: SVGA (1024-768 or more) with high color 24 bits.
      Pointing device:
      • Mouse or compatible devices.
      Web Access:
      • Web registration requires Internet access.
     
    • Access rights on the computer
      • Unity Pro V6.0 needs to have Administrator access right for installing the software.
        For Unity Pro usage User access right are sufficient
        Nevertheless Administrator rights must be used for updating the Hardware catalog (CANopen, DTM)
        PRM DTM requires administrator rights to work correctly.
         
        Note: 
        • -          User must check that all directories used by Unity pro are accessible in read write mode.
                           Check for the Options Management: Options / General / Paths:
      • - Project Path
        - Import / Export file path
        - XVM path
        - Project settings templates path
        - Project settings template file
        - Custom Library path
        - Working drive
        - Log file path
        Check the directory c:\UnityProTemp (Hidden directory) has the following rights: Read, Execute and Write.
         
        • If these paths are not accessible an error message will appear and the requested operation will fail
        • -          As some components are shared, when several instances of Unity Pro are launched, rights access must be the same on all the instances.
Was this helpful?
What can we do to improve the information ?