Technical FAQs

Ask a Question

How can I make use of ISA symbols such as 'solenoid' and 'horn' in my ladder logic and I/O drawings using Proworx 32?

To display an ISA symbol that is tied to an I/O module for use in an I/O Generated Drawing, insert the ISA symbol preceded by a '$' in the first line of the descriptor field
in the documentation editor. For example, '$HORN'.
To use the symbol in ladder logic insert the ISA symbol in the 'ISA symbol' field in the documentation editor. For example, 'HORN'.

Was this helpful?
What can we do to improve the information ?