Technical FAQs

Ask a Question

Can the RS485 port on the Momentum weighing module be used to connect to a different display than the TSX XBT 200 Magelis display ?

No, you cannot connect a different display to the RS485 port. The ISP module uses a proprietary protocol that is intended to provide greater data integrity during data transmission. This is a requirement when the ISP module is used to provide compliance to legal requirements for commercial transactions. One possible solution to using a different display would be to add a Momentum processor on the weighing module and then using one of its ports to communicate to the display.

Was this helpful?
What can we do to improve the information ?