Technical FAQs

Ask a Question

Video: How do you check and see which addresses have been used in a ProWORX 32 project?

Goals and Symptoms

To see which addresses have been used in a ProWORX 32 project.

Causes and Fixes

With your ProWORX 32 project open, click on View then Address Used. This will open the Address Used table. Click on the Rebuild button to update the addresses used.
To view an address type, click the corresponding tab.....0xxxxx, 1xxxxx, 3xxxxx or 4xxxxx.

The Address Used table displays the following information, as noted in the legend:
 

Display Description
Top-left purple square Address is used in logic
Top-right blue square Address is used in the traffic cop
Bottom-left green square Address is used in the Peer Cop
Bottom-right yellow square Address is used in the I/O Scanner
An overlaid C Coil is used in logic
An overlaid D Duplicate coil is used in logic

Was this helpful?
What can we do to improve the information ?