Technical FAQs

Ask a Question

How to create a ProWORX 32 Quantum PLC security password.

Goals and Symptoms

To create a Quantum PLC security password in the ProWORX 32 programming software.

Causes and Fixes

In ProWORX 32 this can be done while Online to the Quantum controller. First open the Configuration Extensions.


Then check off the option for Quantum Security and you will be able to set the PLC Password.

Attachments

Once the PLC Password has been set, users will be prompted to enter a password to get online to the Quantum controller.

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/8b74f9c21d8089e2c12576780058110b/fl_block_5/12.30EC?OpenElement&FieldElemFormat=gif)

Users who enter the wrong password will be rejected and will not be allowed to log onto the Quantum controller.

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/8b74f9c21d8089e2c12576780058110b/fl_block_5/25.4A78?OpenElement&FieldElemFormat=gif)

 
Was this helpful?
What can we do to improve the information ?