Browse FAQs

Is there an AutoConnect feature in Concept?

Published date: 11 February 2019

Issue:
Yes, you can autoconnect in Direct mode from the command prompt.
\concept.exe /C=<Parameter>

Modbus: /C=[x,]MB:m[,ASCII]

x = COM port (1,2,3,4) ) default = 1
m = PLC Node (1 to 247)
ASCII mode. (optional. default = RTU)

Modbus Plus /C=[x,]MBP:[??,]n.n.n.n.

x = MB+ port (0,1)
?? = 2 ASCII characters, ignored in Concept. Used by specific customer tools.
n = MB+ routing (1 to 64)

TCP/IP /C=[x,]MBT:m.m.m.m
/C=[x,]MBP:HostName (Local Host connected to PLCSIM32)

x = Bridge MB+ Index )(0-255)
m = IP Address octet (0 - 255)

Product line    Concept

Environmental  Not applicable

Cause  Improve functionality

Resolution  Not applicable


Legacy KB System (APS) Data: RESL199314 V1.0, Originally authored by DaSo on 07/08/2009, Last Edited by DaSo on 07/08/2009
Related ranges: Concept

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.