Technical FAQs

Ask a Question

Can a brand new M340 BMXP34xxxx CPU be downgraded from V2.0 to V1.0 firmware with the M340 unity loaded so it can be used with UnityXL 3.1?

Yes... you can downgrade a BMXP34xxxx CPU from V2.0 to V1.0.

Was this helpful?
What can we do to improve the information ?