Browse FAQs

Why do I get a Warning message - "version mismatch PLC/program. Not possible to connect to equal" when exporting my Concept project?

Published date: 27 March 2019

Issue
Warning message - "version mismatch PLC/program. Not possible to connect to equal"

Product Line
Concept

Resolution
This warning message would occur if choosing export option "Project with used DFB s (Re-Connect to Equal)". If the PLC and project are not equal, this would cause the Warning message - "version mismatch PLC/program. Not possible to connect to equal". You would need to choose the export option - "Project with used DFB s". If you want to use the export option "Project with used DFB s (Re-Connect to Equal)", you would first need to do a full download so PLC and project are equal. Once the PLC and project are equal, this option should work without any warnings or error messages.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.