Technical FAQs

Ask a Question

What causes a -6001 or -6003 error when installing Vijeo Designer V4.6?

This error is not generated by Vijeo-Designer. It is an error generated by Installshield when the installshield dll`s are out of sync.
To work around this issue, follow the procedure below:

1) Go to C:\Program Files\Common Files\InstallShield\Professional\RunTime
2) Delete or move all contents to some other location (ex. C:\Temp)
3) Re-boot the computer
4) Re-launch Vijeo-Designer installer.

The reason why these dll`s are out of sync is because sometimes other installers of other applications use older or newer versions of installshield. This in turn causes the dlls to be either older or newer. By cleaning out this directory, we can guarantee that the same version of the installshield dlls used by our Installer are used.


Was this helpful?
What can we do to improve the information ?