Technical FAQs

Ask a Question

Video: How do you configure Port Mirroring in a ConneXium TCSESM managed switch?

The first step for setting up port mirroring is a TCSESM managed switch is to log into the switch with admin rights. To do so, open the switch's web page from a internet browser by typing in its IP address in the address field. Please note that the switch and PC need to be on the same subnet. Once on the web page change the user name to admin and use the password private. Then press OK.


In the navigation tree expand Diagnostics and double click on Port Mirroring.



Next choose your Source port (port to be mirrored) and Destination port (port to where the source data will also be sent). Make sure that the enable box is checked.
Finally press Set to write the configuration to the switch.



The following video demonstrates this procedure:
 

Was this helpful?
What can we do to improve the information ?