Technical FAQs

Ask a Question

The cable pinout for a Momentum option module 172JNN21032 Modbus serial RS232 to Magelis XBTGT 1130.



This cable pinout is used in place of the combination of these two cables; XBTZ939 and XBTZ9711.


Was this helpful?
What can we do to improve the information ?