Technical FAQs

Ask a Question

Is it possible to connect to a MB+ network via the Ethernet without using a MB+ to Ethernet Bridge?

This can be done by setting a Client and Server using the MBX Gateway driver on a PC connected to the MB+ network and a remote PC connected to the first PC via the Ethernet.
Note: For information on how to setup the MBX Gateway Client and Server see the resolution entitled "How to connect remotely to a MB+ network via TCP/IP using the MBX Gateway driver"


Was this helpful?
What can we do to improve the information ?