Technical FAQs

Ask a Question

Which Tasks are allowed in the Unity Pro v3.1 XLS software?

In Safety Applications only the MAST task is allowed. FAST/AUX tasks and EVENTS are not allowed because of the predictability of the Safety Application execution.

Was this helpful?
What can we do to improve the information ?