Technical FAQs

Ask a Question

How do you set the IP address to the Ethernet port on the M340 PLC's BMXP34 2020/2030?

The addressing of the Ethernet port is done by the 2 rotary switches on the back of the PLC. There are 4 ways to obtain the IP address:
1. By Stored Device uses applications configured IP address.
2. By BootP Device gets an IP address from a BootP server.
3. By Clear IP Device used default IP address based on the MAC address.
4. By Tens and Ones Rotary Switches Used to define the default device name of the module to obtain an IP address from a DHCP server.


Was this helpful?
What can we do to improve the information ?