Technical FAQs

Ask a Question

What is the maximum number of messages that can be programmed in the 140ESI06210 Quantum ASCII module?

The maximum number of messages that can be programmed in the 140ESI06210 Quantum ASCII module is 255.

Was this helpful?
What can we do to improve the information ?