Browse FAQs

Can you reserve I/O words in the Advantys STB Modbus I/O Image for future use?

Published date: 31 October 2018

The only method of reserving IO data image words is via a new feature introduced in version 2.0 which is called "Virtual Placeholder Modules". This feature will allow you to add future modules and reserve IO data words without effecting the PLC program in the future. This feature is implemented by double clicking on an I/O module and checking off the box "Not Present". Note this option will only be present when configuring a version 2.xx NIM (Network Interface Module).


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.