Technical FAQs

Ask a Question

Why can't I access a Concept IEC program that was loaded to my PLC?

With Concept v2.6, there's an option in the Code Generation Options to "include IEC upload information" when doing the original download to the PLC. This option must be checked off when doing the original download in order to do any future uploads of the IEC information. Unfortunately, there's no other option or procedure to retrieve the IEC upload information.


Legacy KB System (APS) Data: RESL173428 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?