Technical FAQs

Ask a Question

Can I display register data on my logic area in ProWORX Plus, ProWORX NxT, and ProWORX 32?

Yes.
In Proworx32, select a data field in the logic properties for the project.
Once that data has been selected, select apply and OK.


In Proworx NxT select a data field in the network display setup using a custom screen setup.


In Proworx Plus;

  1. Select offline main menu
  2. Utilities
  3. Configuration
  4. Network display setup
  5. Options
  6. Custom setup
  7. Edit
  8. Select a data field
 
Was this helpful?
What can we do to improve the information ?