Browse FAQs

What discrete output functions are supported by the 170AEC92000 Momentum high speed counter base when configured for frequency or period mode?

Published date: 31 October 2018

When the Momentum high speed counter is setup for frequency mode, the discrete outputs can only be configured as "pulse outputs". When the counter is setup for period mode, the discrete outputs can only be configured as "frequency outputs". Please refer to the TSX Momentum 170AEC92000 User Manual (870USE00800) for additional details.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.