Browse FAQs

How can I connect 2 Magelis HMIs and a modem to the TER port on a TSX Micro / Premium?

Published date: 31 May 2019


The diagram below details proposed Unitelway network configuration.
A maximum of 8 slave addresses can be connected to the TER port.

Slave addresses:
Modem Programming connection Adr 1,2 & 3 Configured within Unitelway Driver
Magelis 1 Adr 4 & 5 Set within the TSX SCA 62 Tap box
Magelis 2 Adr 6 & 7 Set within the TSX SCA 62 Tap box


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.