Browse FAQs

Can I alter my RIO cabling without stopping my process?

Published date: 29 March 2019

Issue
Alter RIO cabling without stopping process

Product Line
Modicon

Resolution
No. Alteration of the RIO cabling would result in a loss of termination. Communications to the entire network could be disrupted. It should be noted that a RIO drop module can be unplugged from the network without disrupting communications to the other drops if and only if a Self Terminating F Adapter is installed on that drop cable. Disconnect would then be made at the Self Terminating F adapter (P/N 52-0720-000).


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.