Control power rating on the CM4000 series meter is different than what is stated in the specifications in CM4 manual
Issue Control power rating is different than what is shown in the CM4000 series user manual
Product Line CM4000 Series
Environment
Wiring
Resolution
The control power for the CM4000 series Circuit Monitors is rated for a voltage range of 90-305V ac or 100-300V dc. It was our standard practice to publish these ratings. Recently a change was implemented to mark the circuit monitors with the nominal voltage ranges instead of the maximum range. As a result the meters now show a control power voltage range of 100-277 V ac or 125-250 V dc.
If the customer needs a document with signature for their customer, you can send them the following document from John Straughn below.
Sign up for all the latest solutions, offers and best practices straight to your inbox.
All done!
Thank you for subscribing to updates from Schneider Electric.
We are excited that you have joined the group. You will receive your welcome email soon describing the program and what to expect in the upcoming weeks. Enjoy!