Technical FAQs

Ask a Question

Hardware Note: Issue with the way BCPM processed data in 2 pole and 3 pole configurations

Issue
In firmware versions prior to 1.005 RS and 1.012 OS, there were known issues with the way the BCPM processed data in 2 pole and 3 pole configurations.

Product Line
Branch Circuit Power Meter (BCPM)
DLF-3000

Environment
Firmware Upgrade

Cause
Old firmware

Resolution
Firmware was released on January 18, 2011 to address an issue with the way BCPM processed data in 2 pole and 3 pole configuration. The versions released are 1.005 RS and 1.012 OS. DLF-3000 is used to send the firmware to the meter.

The following link is to the latest firmware for a BCPM:
Branch Circuit Power Meter (BCPM)

Use the following link to download the DLF-3000 software:
DLF-3000 Download

*Reference FA212885 for an example of how to upgrade BCPM firmware.

Was this helpful?
What can we do to improve the information ?