Technical FAQs

Ask a Question

What are the Expansion SnapOn Modbus Registers in ION6200?

Issue
What are the Expansion SnapOn Modbus Registers in ION6200?

Product Line
ION 6200

Environment
ION 6200 Modbus Map

Cause
What are the Expansion SnapOn Modbus Registers in ION6200?

Resolution
These Modbus registers were allocated in the early stages of the ION 6200 product development, but were never implemented.
40500 Expansion, SnapOn 1, 25 regs Expansion, SnapOn 1, 25 regs UINT16 x1 
40700 Expansion, SnapOn 2, 25 regs Expansion, SnapOn 2, 25 regs UINT16 x1

Was this helpful?
What can we do to improve the information ?