Browse FAQs

Filters and Available Nodes are out of order in Active Pager Module (APM) Filter-Setup

Published date: 16 April 2019

Issue
Filters and Available Nodes appear in a random order when viewed in APM Setup

Product Line
APM 6.0, 6.1, 6.2

Environment
APM configuration

Resolution

The following patch corrects ordering (alphabetically, ascending) of all items in the Filter page of APM Setup

*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

Patch Instructions

1. Stop APM and OPC Logger services and shut down the eSolution website if running
2. Remove the PowerLogic.eSolutions.APMSetup.WEB.dll from the [install location]\PLeSolutionsWeb\PLAPMSetupWeb\bin\ folder
3. Place it in a different location as a back up
4. Copy the included dll in the [install location]\PLeSolutionsWeb\PLAPMSetupWeb\bin\ folder
5. Run the Filters_Arrangement batch file
6. Start the APM and OPC Logger service

Legacy KB System (APS) Data: RESL202769 V1.0, Originally authored by MaTh on 06/29/2010, Last Edited by MaTh on 06/29/2010
Related ranges: SMS Add-on


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.