Browse FAQs

What is Disturbance Direction Detection in a Power Monitoring System?

Published date: 24 January 2018

Issue:
What is Distrubance Direction Detection

Product:
ION76XX, ION75XX, ION8XXX, and PM8000

Environment:
Power Metering

Resolution:
Meters with the Disturbance Direction Detection Module can detect faults upstream and downstream of the meter.
The module will give you a confidence level of where a disturbance in the line voltage or line current occurred in regards to the meter’s location.
For an in depth description of the Disturbance Direction Detection module please see the attached document. 
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.