Technical FAQs

Ask a Question

Devices names on ECC21/EGX400 web pages do not match what was entered in WebPageGenerator

Product Line
EGX400
ECC21

Environment
Web Pages

Cause
Certain character combinations cannot be used in WebPageGenerator. When the HTML code is created, the program interprets the characters as HTML code.

Resolution
Replace known non-useable characters.
Use spaces or underscores between letters and numbers.

Characters with known issues
'Z4' is replaced with "return"
'Z5' is replaced with "break; case"

Was this helpful?
What can we do to improve the information ?