Technical FAQs

Ask a Question

How to disable the audible part of a CM alarm in SMS

Issue
Customer does not want an audible alarm in the System Manager Software.

Product Line 
System Manager Software 3.3 and higher

Environment
Alarm settings

Cause
Alarms are audible as a default in SMS

Resolution
1. Go to Setup > Devices Routing.
2. Highlight the device and click Configure.
3. Go to the Onboard Alarms/Events tab. Enable the alarm and configure setpoints/delays.
4. Press PC Task then click Severity. Take the check mark out of the audible box for the level alarm you are using. This alarm level will no longer cause a sound.

Was this helpful?
What can we do to improve the information ?