Technical FAQs

Ask a Question

What is the part number of the quickstart kit for the CM4000?

Issue
Part number needed for the quickstart kit for the CM4000 meter.

Product Line
CM4000 Series Meters

Environment
Metering & Power Monitoring

Cause
The quickstart kit permits the temporary installation of CM4000 series meters for testing.

Resolution
The orignal class number 3070 with a part number of CM4000QSK is obsolete and an updated replacement part number is not offered by Schneider electric.

For further information, the instruction bulletin can be found at the following link: http://www.schneider-electric.us/en/download/document/63230-300-220/
Was this helpful?
What can we do to improve the information ?