Technical FAQs

Ask a Question

How many registers are available for logging with the extended memory option for the CM2?

Product Line:
CM2000

Environment:
Logging

Resolution: 

The 512 KB CM2000s have 313,344 registers available.
The 1024 KB CM2000s have 575,488 registers available.

Was this helpful?
What can we do to improve the information ?