Technical FAQs

Ask a Question

ProWORX NxT has an "Instruction Editor" for looking at values inside of an instruction. When converted to Unity 7+, is this functionality available for the 984LL instructions?

Yes. It is available when ON-LINE. Select the instruction, right click and select "Show Instruction".

Was this helpful?
What can we do to improve the information ?