Technical FAQs

Ask a Question

Does Schneider offer an API tool for Modbus TCP?

Yes. The TCP Open Library is available for Premium only. Both hardware and software components are needed.
The part numbers are TSXETY5103 for the hardware module and TLXCDTCP50M for the software. ( both need to be purchased separately )


Legacy KB System (APS) Data: RESL212126 V1.0, Originally authored by DiSa on 07/24/2013, Last Edited by DiSa on 07/24/2013
Related ranges: Modicon Premium
Was this helpful?
What can we do to improve the information ?