Technical FAQs

Ask a Question

Is there a way to update Initial Values with current values on the M340 by using a System Bit ?

Yes. This is accomplished by toggling %S94 to 1 , and then back to 0. If the update is successful %S96 will have a value of one (1).




R-2262018


Was this helpful?
What can we do to improve the information ?