Browse FAQs

Connexium Network Manager fails to identify the TCSESM extended switches and returns a PSM error.

Published date: 11 July 2019

Issue

'Connexium Network Manager' fails to identify the TCSESM extended switches and returns a PSM error.

Product Line

TCSEAZ03P002F10 version 1.0

Environment
Windows 7, Windows 8

Resolution

Using the 'Connexium Network Manager' software on a Windows XP PC with the Multi-language pack
installed for Chinese character support, or on a PC that has the Chinese version of Windows XP installed,
returns a PSM error. This problem occurs when an 'ESDiscovery' is performed on a network that contains
the TCSESM Extended switch. The TCSESM Extended switch also get represented in the 'Map' tab with
an incorrect icon.

This issue has been fixed in version 1.0.01.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.