Technical FAQs

Ask a Question

What is the cable pinout for the Com 1 RS485 2 wire between two Magelis XBTGC / XBTGT OR HMIGTO?


XBTGC XBTGC
XBTGT XBTGT


1--| |--1
|----------------------------| (jumped on both sides and connected across)
3--| |--3


2--| |--2
|----------------------------| (jumped on both sides and connected across)
7--| |--7



4--| |--4
| | (jumped on both sides only)
8--| |--8



6--| |--6
| | (jumped on both sides only)
9--| |--9


Legacy KB System (APS) Data: RESL205214 V2.0, Originally authored by MiMe on 04/29/2011, Last Edited by HaKa on 05/09/2013
Related ranges: Magelis XBT G
Was this helpful?
What can we do to improve the information ?