Technical FAQs

Ask a Question

Is there a way with the Advantys Modbus OTB to read the data as either MSW (Most Significant Word) or LSW (Least Significant Word)?

Goals and Symptoms

To show how to set up the configuration to read either right to left or left to right.

Causes and Fixes

Yes, you can set up the OTB to read left to right or right to left (MSW or LSW). Below is how you set it up.

Theses are in 32 bit format and the default is MSW/LSW


first highlight the OTB module


Double click on the module and the following screen will appear.



Select the OPTIONS tab



From the Transfer Format go to the pull down and select from the following.


 

Legacy KB System (APS) Data: RESL192876 V2.0, Originally authored by DiSa on 10/01/2008, Last Edited by BrWa on 05/01/2012
Related ranges: Modicon OTB
Was this helpful?
What can we do to improve the information ?