Technical FAQs

Ask a Question

What Advantys NIM's can talk to the ATV31 Altivar Drive and what version are they compatible with?

The following are the Type of NIM's and part numbers along with the minimum version that is required.


Legacy KB System (APS) Data: RESL177890 V3.0, Originally authored by DiSa on 09/21/2009, Last Edited by BrWa on 10/19/2012
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?