Browse FAQs

Why does Concept detect Momentum IO Bus nodes as generic IO Bus modules?

Published date: 31 October 2018

Goals and Symptoms

Detection of Momentum IO bases on IO bus

Facts and Changes

Concept monitoring on-line

Causes and Fixes

Concept programming software will detect all Momentum modules configured on IO Bus using an equivalent generic IO Bus Code Identifier and not the specific Momentum module type. For example the 170ADO53050 when configured as an IO Bus node will be detected on-line as a IOBUS-0101 and not a ADO53050.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.