Browse FAQs

Does Advantys STB have a High Density DC I/O module?

Published date: 16 April 2019

Issue:
High density Advantys I/O modules 

Product Line:
Advantys STB

Environment:
Advantys Configuration Software

Cause:
Looking for high density module for the Advantys STB line.

Resolution:

Yes. Two new High Density 16 Pt, DC Input and Output modules are now available for the Advantys® STB distributed I/O platform. They will provide higher I/O count for each automation island and significantly reduce the size and cost of a system using the same quantity of I/O.
The data sheets for these two modules is attached below.


STBDDO3705 HiDensity Output.zipSTBDDI3725  HiDensity Input.zip

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.