Technical FAQs

Ask a Question

Can I save my program to flash memory using Unity Pro?

Yes. Unity processors support for save to flash is available by selecting from the Unity menu bar, PLC -> Project Backup. Select the option desired: Backup Compare, Backup Restore, Backup Save or Backup Clear.

Was this helpful?
What can we do to improve the information ?